Press Releases
Industrial Shields PLCs and panel PCs now available at RS Components
Extensive portfolio leveraging Arduino, Hummingboard and Raspberry Pi boards delivers open-source advantages on ready-to-use, approved hardware
Malaysia, 29 September 2015:
RS Components (RS), the trading brand of Electrocomponents plc (LSE:ECM), the global distributor for engineers, is now stocking the Industrial Shields range of PLCs and panel PCs, which combines the advantages of open-source hardware (OSH) with the reliability of industrial-standard products.
In the past few years the flexibility of open-source development boards has eased the design process for electronic engineers, enabling faster prototyping for cutting-edge applications, especially in the Internet of Things (IoT) space. “Our new distribution agreement with Industrial Shields brings this flexibility to industrial engineers with a series of ready-to-install open-source industrial products,” said Paolo Carnovale, Global Category Marketing Manager for Automation & Control at RS. The Industrial Shields PLCs and panel PCs are based on the most popular open-source developments boards, such as Arduino, Raspberry Pi and Hummingboards, and can be programmed exactly in the same way. This unique characteristic allows engineers to go from prototype to industrialisation using the same flexible programming code.
The PLC portfolio comprises ARDBOX compact PLCs based on the Arduino Leonardo board, and M-DUINO Ethernet PLCs based on the Arduino Mega board. All operate from a supply voltage of 12-24V DC, and can be programmed and monitored via the Arduino IDE platform. ARDBOX compact PLCs are available in two different versions with up to 20 I/Os giving a choice of digital, analogue and relay outputs. The M-DUINO series offers five different versions with up to 58 I/Os. All units support I2C communication allowing I/O expansion by connecting multiple units together. USB, RS232 and RS485 communication ports are also provided.
The panel PCs are open-source programmable 10.1-inch capacitive touchscreens, available in three different versions. HummTOUCH Android and HummTOUCH Linux give a choice of popular operating systems running on the Hummingboard ARM-based single-board computer. TOUCHBERRY Pi, based on the Raspberry Pi, runs the Raspbian Linux operating system. All the usual communication ports including Ethernet, USB, SPI Serial TTL and I2C are provided, and the units can be programmed quickly via the USB port using the Arduino IDE that is based on Processing.
About RS Components
RS Components and Allied Electronics are the trading brands of Electrocomponents plc, the global distributor for engineers. With operations in 32 countries, we offer more than 500,000 products through the internet, catalogues and at trade counters to over one million customers, shipping around 44,000 parcels a day. Our products, sourced from 2,500 leading suppliers, include electronic components, electrical, automation and control, and test and measurement equipment, and engineering tools and consumables.
Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2015 had revenues of £1.27bn.
For more information, please visit the website at www.rs-online.com.
Further information is available via these links:
Twitter: @RSElectronics; @alliedelec; @designsparkRS
RS Components on Linkedin
http://www.linkedin.com/company/rs-components
Relevant Links:
Electrocomponents plc
www.electrocomponents.com
RS Components
www.rs-online.com
DesignSpark
http://www.designspark.com