• Published 27 Oct 2026
    • Last Modified 27 Oct 2026
  • 10 min

What Is a Tachometer? Types, Function & Working Principle

RS marketing banner
What Is a Tachometer? Types, Function & Working Principle

A tachometer is an instrument that measures the rotational speed of a shaft, disc, motor, or other rotating components, typically expressed in revolutions per minute (RPM). The primary tachometer function is to help operators monitor machine speed, verify that motors and engines are running within their rated speed range, and identify speed-related faults before they lead to equipment damage or unplanned downtime.

Tachometers are widely used in automotive, industrial, maintenance, manufacturing, and engineering applications wherever accurate RPM measurement is required.

What Does a Tachometer Measure? (Tachometer Function)

A tachometer measures the rotational or angular speed of a rotating component, such as a motor shaft, engine crankshaft, fan assembly, spindle, pulley, or gear. The reading is most commonly displayed in revolutions per minute (RPM), although some instruments can also display revolutions per second (RPS), frequency (Hz), or linear surface speed depending on the model and measurement method.

While tachometers are primarily used to measure rotational speed, some contact tachometers can also measure linear surface speed using a wheel attachment. Depending on the instrument, the result may be displayed in units such as metres per minute (m/min) or feet per minute (ft/min).

The function of a tachometer extends across several practical applications:

  • Process control: In manufacturing and automation, maintaining the correct RPM is critical for consistent product quality. A tachometer confirms that a motor or drive is running at the intended speed and allows operators to adjust it if necessary.
  • Speed monitoring: Engines, motors, turbines, and spindles all have rated speed ranges. Running outside these ranges (whether too fast or too slow) can cause overheating, mechanical stress, or reduced output. A tachometer provides real-time feedback to keep equipment within its safe operating envelope.
  • Fault diagnosis: An unexpected drop or spike in RPM can signal a worn belt, a bearing failure, or an electrical fault in the drive system. Tachometers help maintenance teams identify these issues early before they escalate into unplanned downtime.
  • Quality assurance: In precision machining, RPM directly affects surface finish and dimensional accuracy. A tachometer is used to set and verify cutting speed before a machining operation begins.
  • Motor speed feedback: Tachometers are also used to feed rotational speed data back to motor controllersfor closed-loop speed regulation, ensuring that the motor maintains the commanded speed under varying loads.

How Does a Tachometer Work? (Working Principle)

The working principle of a tachometer is based on detecting recurring signals generated by a rotating object and converting those signals into rotational speed.

As the shaft or rotating component turns, the sensor detects pulses associated with the rotation. The tachometer counts these pulses over a precisely timed interval and calculates the corresponding RPM.

The basic relationship is:

RPM = Number of pulses counted ÷ Measurement time (in minutes)

For example, if a tachometer counts 500 pulses in 30 seconds, the RPM is 500 ÷ 0.5 = 1,000 RPM.

Depending on the instrument and sensor arrangement, there may be one pulse per revolution or multiple pulses per revolution. The tachometer uses the known pulse relationship to calculate RPM accurately.

The method used to generate the pulses varies depending on the tachometer type:

  • Contact tachometers: Generate pulses through direct mechanical contact with the rotating component.
  • Optical or laser tachometers: Detect reflected light from reflective tape attached to the rotating surface.
  • Magnetic tachometers: Detect changes in the magnetic field or passing ferromagnetic targets.

Regardless of the sensing method, the tachometer processes the incoming pulse signal electronically and converts it into a rotational speed reading. How does a tachometer read RPM accurately? By consistently detecting the intended pulse pattern and precisely timing the measurement interval.

Because the signal-generation method determines the instrument type, understanding the working principle is the clearest starting point for choosing the right tachometer. The types and their differences are covered in the next section.

Types of Tachometers

The different types of tachometers can be grouped by how they make contact with the rotating object and by how they display their readings.

Contact Tachometers

Contact tachometers measure RPM by physically touching the rotating shaft or surface with a probe or wheel tip attachment. The attachment rotates with the shaft, and the instrument counts the rotations electronically to calculate RPM.

Advantages:

  • Simple operation
  • No reflective tape required
  • Suitable for direct-access applications
  • Can often measure linear surface speed as well as RPM

Limitations:

  • Requires physical access to the rotating component
  • Not suitable for very high-speed shafts
  • Unsuitable for hot or hazardous surfaces
  • Measurement can be affected by slipping between the tip and shaft surface

Non-Contact (Laser/Optical) Tachometers

Non-contact tachometers use a laser or optical beam to detect rotational movement without touching the shaft. A reflective marker is typically attached to the rotating object. Each time the reflective target passes through the beam, the instrument detects a pulse and calculates RPM.

Advantages:

  • No physical contact required
  • Suitable for high-speed applications
  • Safer around rotating machinery
  • Useful for inaccessible or enclosed equipment

Limitations:

  • Requires reflective tape or a suitable target
  • Sensitive to alignment and measurement conditions

Non-contact tachometers are widely used in motor maintenance, fan balancing, generator testing, and machinery diagnostics.

The photoelectric sensing principle used in these instruments is covered in our guide to types of photoelectric sensor.

Combination Tachometers

Combination tachometers offer both contact and non-contact measurement modes within a single instrument.

They typically include interchangeable measuring tips and wheels for contact measurements while also supporting optical or laser RPM measurement.

Combination instruments are popular with maintenance technicians because they can adapt to a wider range of measurement situations without requiring multiple instruments.

Analogue Tachometers

Analogue tachometers display RPM using a moving pointer and graduated dial. They are commonly used where operators need to observe speed trends continuously rather than record precise numerical values.

Advantages:

  • Easy to observe changing speed conditions
  • Instant visual indication of RPM changes

Limitations:

  • Lower reading precision than digital instruments
  • Limited additional functionality

Digital Tachometers

Digital tachometers display the RPM reading as a number on an LCD or LED screen and are the most common type in current use.

Advantages:

  • High readability
  • Greater measurement precision
  • Additional features such as max/min hold, data logging, and memory functions

Limitations:

  • Require battery power
  • Can be more sensitive to harsh operating environments depending on design

How to Use a Tachometer to Measure RPM

The procedure for using a tachometer differs depending on whether you are using a contact or non-contact instrument.

How to use a contact tachometer:

  1. Select the correct tip: Choose a flat or conical rubber tip for small-diameter shaft ends, or a wheel attachment for longer shafts where rolling contact is preferred.
  2. Check access and safety: Confirm that the shaft is accessible and that you can hold the probe steadily against it without being exposed to any hazard from nearby rotating parts.
  3. Turn on the tachometer: Switch the instrument on and ensure it is set to contact mode if the model has selectable modes.
  4. Apply the tip: Press the tip firmly against the centre of the rotating shaft end or surface and hold it steady. Maintain consistent pressure to prevent slipping, which will produce an inaccurate reading.
  5. Read the RPM: Wait for the reading to stabilise on the display, then note the RPM value. On digital models with max/min hold, trigger the hold function to capture the reading.

How to use a non-contact tachometer:

  1. Prepare the shaft surface: Clean the surface of the rotating shaft or disc where the reflective marker will be applied.
  2. Apply reflective tape: Attach one strip of reflective tape to the shaft surface. One strip per revolution is standard, giving one pulse per revolution. Ensure the tape is flat and secure.
  3. Turn on the tachometer: Switch the instrument on and set it to non-contact mode if applicable.
  4. Aim the laser: Point the laser at the reflective tape from the recommended distance (typically between 50 mm and 500 mm), depending on the model. Consult the instrument manual for the rated measurement distance.
  5. Trigger the measurement: Hold the laser steady while the shaft rotates and trigger the measurement. Wait for the reading to stabilise, then note the RPM value.

Safety note: When using any tachometer near rotating machinery, maintain safe working distances and keep clothing, cables, and other items away from moving parts. Never direct a laser beam at your eyes.

Common Causes of Tachometer Measurement Errors

Several factors can affect the accuracy and repeatability of tachometer measurements. Understanding and addressing these issues can help ensure more reliable results:

  • Slipping contact wheels or measuring tips: When using a contact tachometer, any slipping between the measuring wheel and the rotating surface can result in inaccurate speed readings. Maintaining consistent contact throughout the measurement helps minimise this source of error.
  • Dirty, damaged, or poorly attached reflective tape: For non-contact tachometers, reflective tape must be clean, intact, and securely attached to the rotating component. Damaged or poorly positioned tape can prevent the instrument from accurately detecting each rotation.
  • Poor laser alignment: Accurate measurements depend on proper alignment between the tachometer and the reflective target. Misalignment can reduce signal quality and lead to unstable or incorrect readings.
  • Excessive vibration: Vibration from machinery or surrounding equipment can interfere with measurement stability, particularly when taking readings on high-speed rotating equipment.
  • Ambient light interference: Strong ambient lighting, especially direct sunlight or intense artificial lighting, can sometimes interfere with the optical sensor and affect measurement accuracy.
  • Incorrect measurement distance: Non-contact tachometers typically operate within a specified measurement range. Taking readings outside the recommended distance can reduce detection reliability and measurement accuracy.
  • Unstable instrument positioning: Holding the instrument unsteadily or changing its position during measurement can produce inconsistent readings. Maintaining a stable measuring position helps improve repeatability.

Verifying the testing setup and addressing these potential issues before taking measurements can significantly improve accuracy and reliability.

Common Tachometer Applications

Tachometers are widely used across industrial, maintenance, and engineering environments to measure rotational speed and verify equipment performance.

Common applications include electric motor testing and maintenance, generator commissioning and inspection, fan and blower performance monitoring, conveyor system maintenance, and pump diagnostics. They are also frequently used for monitoring machine tools and CNC spindles, evaluating turbine performance, conducting automotive engine diagnostics, maintaining HVAC equipment, and supporting manufacturing process control activities.

Because of their versatility, tachometers are valuable tools for engineers, maintenance technicians, reliability specialists, and condition-monitoring teams responsible for maintaining rotating equipment.

Contact vs Non-Contact Tachometers

Understanding the different types of tachometers starts with the fundamental distinction between contact and non-contact models, which each offer distinct advantages depending on the application and operating environment.

Feature
Contact Tachometer
Non-Contact Tachometer
Physical contact requiredYesNo
Suitable for inaccessible shaftsNoYes
Reflective tape requiredNoUsually
High-speed applicationsLimitedBetter suited
Safety around rotating equipmentLowerHigher
Surface speed measurementOften supportedGenerally not supported

Compared with contact models, non-contact tachometers generally provide safer operation around rotating machinery and are often preferred when access, speed, or safety considerations make direct contact impractical.

While non-contact tachometers are widely used for rotational speed measurement, contact tachometers remain a practical choice for applications requiring direct measurement or surface-speed calculations.

Choosing a Tachometer

Before selecting a tachometer, consider the following factors:

  • Contact or non-contact: Contact tachometers suit accessible, lower-speed shafts where physical contact is safe. Non-contact tachometers are the better choice for high-speed, high-temperature, or hard-to-reach shafts.
  • RPM range: Verify that the tachometer's maximum and minimum RPM range covers the speed of the component you need to measure. Exceeding the upper limit will produce an error or no reading.
  • Accuracy: For quality assurance or precision alignment tasks, choose a model with low measurement uncertainty, typically expressed as a percentage of reading. Lower percentage values indicate higher accuracy.
  • Data logging and memory: If you need to record speed over time or capture peak and minimum values, choose a model with built-in logging or max/min memory hold functions.
  • Attachments and accessories: For contact tachometers, check that suitable tip and wheel attachments are included or available separately.

Browse the full RS Malaysia range of tachometers and tachometers for generators to find the right instrument for your application.

Frequently Asked Questions About Tachometers

Be the first to know about our latest products and offers

Email address

The personal information you provide to us when signing up to this mailing list will be processed in line with the Privacy Policy