• Published 27 Nov 2024
    • Last Modified 27 Nov 2024
  • 8 min

Explore Different Chisel Types and Their Applications

Chisels Guide

Choosing the right chisel can be challenging with so many options available. This comprehensive guide explores various types of chisels including woodworking, concrete, and cold chisels. It offers practical advice on how to use each type effectively, ensuring you select the best tool for your specific project needs. Additionally, discover popular brands that provide quality chisels suited for both professionals and DIY enthusiasts.

What are Chisels?

Chisels have been essential tools in various forms for thousands of years, playing a crucial role in craftsmanship across multiple industries. Despite the wide array of chisel types available today, the fundamental purpose of a chisel remains unchanged: it is designed to carve, cut, and shape hard materials such as wood, stone, and metal.

A chisel is a hand-held tool characterised by its sharp cutting edge, which is specifically engineered for precision work. These tools are indispensable in workshops and toolkits, frequently utilised by both professionals and DIY enthusiasts in woodworking, masonry, and metalworking applications.

Chisels are crafted from various materials, including chrome vanadium steel and forged steel. The choice of material affects the chisel's durability and performance. Smaller chisels excel at intricate tasks in woodworking, while larger chisels are ideal for removing substantial sections of material.

Types of Chisels

Chisels are versatile tools that come in various types, each designed for specific applications. Understanding the different types of chisels is essential for selecting the right tool for your project. Below, we detail some of the most common chisel types and their uses.

Brick Chisels

Brick Chisels

Brick chisels, also known as bolster chisels, are designed primarily for cracking rather than cutting through hard materials. They feature a wide, flat blade that allows for effective splitting of masonry blocks and bricks.

These chisels are user-friendly, provided that the blade remains flat during the cracking process. Many brick chisels come equipped with molded handguards, ensuring a secure grip while in use. Their robust design makes them ideal for various masonry tasks, including shaping and splitting bricks.

Masonry Chisels

Masonry Chisels

Masonry chisels are essential tools for cutting bricks, cement blocks, and cinders. They are also effective for removing excess mortar from joints. Stonemasons’ chisels typically have dull heads designed for breaking and wedging materials. This type of chisel is often heavier and features a handle designed to protect the user from impact.

Masonry chisels can be used manually or attached to hammer drills or jackhammers during demolition work. For heavy-duty tasks, hydraulic rams or falling weights may be employed to enhance chiselling efficiency.

Concrete Chisels

Concrete Chisels

Concrete chisels are specifically designed for making precise cuts in concrete. These chisels usually feature a sturdy handle and a strong bevelled edge blade that allows them to cut through concrete effectively when struck with a hammer or mallet.

How to Use a Concrete Chisel

To chisel concrete effectively, follow these steps:

  1. Positioning: Loosely grip the chisel and carefully place the point against the area of concrete you wish to remove.
  2. Striking: Firmly hold a small sledgehammer or mallet and tap the head of the chisel with controlled force. Use the point of the chisel to chip away at the concrete.
  3. Blade Alignment: Adjust the chisel so that the full width of the blade rests against the concrete, ensuring that the bevel is parallel to the surface.
  4. Continued Striking: Continue striking the head of the chisel until you have removed the desired amount of concrete.

Cold Chisels

Cold Chisels

Cold chisels are made from tempered steel and are specifically designed for cutting cold metals—those not heated by torches or other devices. Unlike standard woodworking chisels, cold chisels have a less acute angle on their cutting edge, providing strength over sharpness.

Common types of cold chisels include:

  • Flat Chisel: The most commonly used type for cutting bars and rods, reducing surfaces, and cutting sheet metal.
  • Cross Out Chisel: Designed for creating grooves and slots; features a narrow blade positioned behind the cutting edge for clearance.
  • Round Nose Chisel: Used for creating semi-circular grooves, particularly useful in applications like oil ways in bearings.
  • Diamond Point Chisel: Ideal for removing debris from corners and hard-to-reach areas.

Woodworking Chisels

Woodworking chisels serve multiple purposes in crafting fine furniture and detailed woodwork. Given the variety of subtypes available, it is crucial to select the right chisel for your specific needs.

Smaller woodworking chisels excel at intricate detailing, while larger ones are better suited for removing substantial amounts of wood. It is common to use both large and small chisels within a single project; larger chisels can tackle initial cuts before smaller tools refine details.

For durability, choose woodworking chisels with handles featuring metal striking caps to withstand repeated impacts. Bench chisels are among the most widely used varieties due to their versatility, while socket handle chisels offer enhanced durability against heavy blows.

Woodworking Chisels

Key types of woodworking chisels include:

  • Bench Chisels: Versatile tools suitable for various applications; they are commonly kept within easy reach on workbenches.
  • Mortise Chisels: Characterised by thick blades ideal for making straight cuts; perfect for creating mortises and joints.
  • Paring Chisels: Long blades designed for cleaning grooves and removing material from tight spaces.

How to Use a Chisel

Using a chisel effectively requires careful consideration of the type of chisel best suited for your specific task, as well as factors such as size and blade shape. Proper technique and preparation are essential for achieving accurate results and ensuring safety during the chiselling process.

  1. Selecting the Right Chisel: Before beginning any project, it’s crucial to select the appropriate chisel based on the material you will be working with. Different chisels are designed for various applications, including woodworking, masonry, and metalworking. Additionally, consider the size of the chisel and the shape of its blade, as these factors can significantly impact your work's precision and efficiency.
  2. Preparing Your Chisel: Start by inspecting your chisel to ensure it is in optimal condition. Use a square to check the flatness of the blade; a warped blade can lead to inaccuracies. If necessary, sharpen the chisel using a honing stone or grinder to maintain a sharp edge, which is vital for effective chiselling.
  3. Measuring and Marking: Once your tool is ready, use a ruler and carpenter’s square to measure the area of wood or other materials that need to be removed. Mark this area clearly with a pencil or chalk to guide your chiselling. This preparation helps you stay within the desired dimensions while working.
  4. Securing Your Workpiece: Clamp the material securely to your workbench or use a vice to ensure stability during chiselling. A stable workpiece minimizes movement and enhances safety.
  5. Chiselling Wood: When chiselling wood, position the chisel at a 90-degree angle to create an initial indentation. Strike the chisel gently with a wooden mallet, ensuring that the bevelled edge is facing toward the wood surface. Follow these steps:
    • Indentation: Create a small indentation in the wood by striking the chisel.
    • Chipping Away: Begin running the chisel along the grain of the wood, carefully chipping away material until you reach your desired depth.
    • Controlled Strikes: Make sure to strike away from your body and remove only small amounts of wood with each hit to maintain control and precision.
    • Finishing Touches: For intricate tasks, use paring chisels that allow for gradual smoothing and removal of surface layers. Keep one hand on the blade for guidance while using your other hand on the handle.
  6. Using Masonry Chisels: Masonry chisels are designed for scoring, trimming, or shaping materials like brick and stone. Selecting a masonry chisel with an appropriate shape and width is crucial for achieving clean cuts. To use a masonry chisel effectively:
    • Marking: Clearly mark the area you intend to chisel using pencil or paver’s chalk.
    • Setting Up: Position the masonry chisel at a perpendicular angle (90 degrees) against the material.
    • Scoring: Firmly strike down in the centre of your scoreline with a mallet, repeating until you achieve an even break.
  7. Maintenance Tips: Regardless of the type of chisel you are using, keep a honing stone nearby to sharpen your tool as needed during work sessions. Regularly sharpening ensures that you maintain cutting efficiency throughout your project. Additionally, consider using a grinder for initial sharpening before honing for finer details.

Types of Materials Used in Chisel Manufacturing

  1. High-Carbon Steel:
    • High-carbon steel is a popular choice for chisels due to its excellent edge retention and ability to be sharpened to a fine point. It offers a good balance of hardness and toughness, making it suitable for various applications.
  2. Alloy Steel:
    • Alloy steels, which include elements like chromium and vanadium, enhance the chisel's strength and resistance to wear. These chisels are often used in heavy-duty applications where durability is paramount.
  3. Beryllium Copper:
    • Some chisels are made from beryllium copper, particularly those used in environments where sparks could ignite flammable materials. This non-sparking material is essential for safety in specific industries.
  4. Stainless Steel:
    • Stainless steel chisels resist rust and corrosion, making them suitable for use in humid environments or where exposure to moisture is common.

How to Keep Your Chisels Sharp and Effective

Proper maintenance of your chisels is vital for ensuring their longevity and performance. Regular care not only keeps them sharp, but also enhances safety during use. Here are some essential maintenance tips to keep your chisels in top condition.

Regular Sharpening

  • Why Sharpness Matters: A sharp chisel requires less force to cut through materials, reducing the risk of slips that can lead to injuries.
  • Sharpening Techniques: Use a whetstone or sharpening jig to maintain the edge of your chisel regularly. For more significant damage, consider using a grinder before honing with finer stones.

Cleaning Your Chisels

  • Remove Debris: After each use, clean your chisels with a soft cloth to remove wood shavings or dust that can cause corrosion.
  • Rust Prevention: Apply a light coat of oil (like mineral oil) on the blade after cleaning to prevent rust formation.

Proper Storage

  • Safe Storage Solutions: Store chisels in a protective case or roll that prevents blades from coming into contact with other tools. This will help maintain their sharp edges.
  • Avoid Humidity: Keep your chisels in a dry environment to prevent rust and corrosion.

Safety Practices When Using Chisels

Wear Appropriate Safety Gear

  • Protective Eyewear: Always wear safety goggles or glasses to shield your eyes from flying debris.
  • Gloves: Use gloves designed for grip; while ensuring they do not hinder dexterity.

Maintain a Clean Work Environment

  • Clutter-Free Workspace: Ensure your work area is tidy and free from obstacles that could cause trips or falls.
  • Good Lighting: Work in well-lit conditions to see clearly what you’re doing and avoid mistakes.

Use Sharp Tools

  • Dull vs. Sharp Chisels: A dull chisel requires more force and increases the risk of slipping. Always ensure your chisels are sharp before starting work.

Secure Your Workpiece

  • Clamping Techniques: Use clamps or vices to secure your workpiece firmly on the bench, preventing movement during chiselling.

Popular Brands

Facom Chisels

Facom

From cold chisels to general-purpose chisels, browse the full range of chisels from Facom.

Shop Now

RS PRO Chisels

RS PRO

Browse the full range of chisels available from RS PRO, our in-house brand, and shop online today.

Shop Now

Bahco Chisels

Bahco

Shop the full range of Bahco chisels with RS and discover the ideal tool to meet your requirements.

Shop Now

Irwin Chisels

Irwin

Irwin chisels are available in a range of different types and sizes to suit varying projects. Shop online today.

Shop Now

Be the first to know about our latest products and offers

Email address

The personal information you provide to us when signing up to this mailing list will be processed in line with the Privacy Policy