Recently searched
      • Published 7 May 2024
      • Last Modified 14 May 2024
    • 12 min

    Network Switches - A Complete Guide

    Find out more about how network switches are used, how they work, and what types are available in our guide.

    In this guide, we’ll take a closer look at the most important aspects of network switches, give an overview of how they work as part of a wired internet or intranet setup, and identify what sorts of additional features or benefits the various models of ethernet switch might provide.

    What is a Network Switch?

    When asking what is a network switch, the most straightforward answer is that it’s a type of wired hub device, chiefly used for connecting multiple people and devices to a given computer network.

    In the context of domestic, commercial or industrial computer networking and connectivity, the main role of network switches is to physically link online resources and devices through a single multi-port entry/exit point. Users connected to the same network via a switch can then be granted access to share some or all of the resources and devices on that network.

    Examples of the sorts of resources commonly found wired together through network switches might include:

    • Any incoming internet connections, usually via a router
    • Numerous types of external storage and file-sharing modules, such as high-capacity hard drives or server arrays
    • A wide range of key hardware and peripherals - desktop computers, laptops, games consoles, smart TVs, UPS power suppliesprinters and more

    Network switches are often referred to as an ethernet switch or LAN switch (Local Area Network). The latter name reflects the fact that they typically rely on cabled connections to support networking activities across a relatively limited physical space, such as a single office.

    How Does a Network Switch Work?

    If you are looking to gain a fuller understanding of exactly how an Ethernet switch works, it’s important to be aware of the various types available. We will touch on this in more depth over the following sections, but for now, we’ll focus on the most basic answer to the question, ‘what does an internet switch do?’

    A switch deployed in a computer network provides a single point of wired connection for numerous individual devices and resources. Data, online connectivity and more can then be shared between some or all the users on that network, and some models allow these connections to be managed and controlled via an onboard software interface.

    At its simplest, a network switch can be considered as a large USB hub, but one specifically made to accept ethernet or RJ45 cables, enabling multi-device sharing of a single wired internet/data connection.

    A standard internet router will likely include at least one built-in ethernet port, but probably not more than two or three for midrange models. To provide a far more robust connectivity solution that allows you to hook in multiple devices and resources - thus creating a more complex Local Area Network, or LAN – you will need to add a network switch.

    Network switches are typically attached directly to a router or server, and their key physical feature is providing a greater number of ports for plugging in additional ethernet cables. The main factor in deciding which type and model of LAN switch to buy will be the demand created by the size and scope of the network you wish to connect through it.

    Accordingly, the number of ethernet ports a given switch provides can range from as few as three, up to 50 and beyond. Where heavy-duty industrial network switches are needed, it’s even possible to find versions offering 100 or more, although these are considerably less common.

    What are the Different Types of Network Switches?

    There are many different types of network switches available, each best suited to different applications. The various types of network switch include:

    Stackable Network Switch

    A stackable switch is one that can be used either as a fully standalone hub or combined with multiple other stackable switches to offer an even greater range of connectivity options. When combined, stackable versions are typically designed to perform and respond as a single large and complex switch, just with the combined port count of however many units are connected together.

    Unmanaged Network Switch

    This tends to be the most basic type and effectively functions as an easy way to add more ethernet ports to your setup. Unmanaged switches don’t usually require any further input from the user beyond hooking up their devices via ethernet cables, and as such are often referred to as ‘plug and play’ or a simple LAN switch. These switches are often used in small offices or commercial environments where precise network control is not as crucial.

    Managed Network Switch

    These switches are used for greater control and advanced functionality. Managed network switches offer a built-in dashboard or similar interface, often displayed through a connected web browser. This provides admin-level users with a suite of tools for monitoring and tweaking various aspects of the network configuration as traffic flows through it.

    Depending on the model in question, options might include anything from access privileges, port mirroring and redundancy, to data transfer rates (port speed), device prioritisation and more. Managed network switches can either be designed as a fully manual switch or a smart switch. The former tends to be the most versatile and is ideal for complex networking requirements (server and enterprise-level setups), while smart switches are usually more user-friendly but provide a limited range of configuration options.

    PoE Network Switch

    Regardless of whether you opt for a managed or unmanaged networking hub, you may also choose a PoE or ‘Power over Ethernet’ switch.

    These models enable power to be transferred to compatible devices via connected RJ45 cables, as opposed to just data. If your network includes several PoE-enabled devices, choosing a switch with this feature included can result in a far neater and more flexible solution, dramatically cutting down on excess cabling (notably to wall sockets), and enhancing overall LAN scalability and reliability.

    Please note that not all hardware is intrinsically PoE compatible – you will need to check the specifications for each device you wish to connect.

    What is the Difference Between Network Switches and Routers?

    When it comes to router vs switch, many people often confuse these closely related pieces of hardware. In practice, though, the fundamental difference between a switch and a router is fairly straightforward once you understand what a switch does. As we’ve already covered, a switch allows multiple devices on the same network to communicate with each other.

    A router, meanwhile, allows multiple different networks to communicate with one another. This is the role played by a domestic ISP-supplied Wi-Fi router, for example - it communicates with external networks to deliver an internet connection into the property from outside. A network switch cannot do this. Instead, it exists to provide greater versatility and flexibility on the network a router brings in.

    The confusion between routers, switches and hubs typically arises because some hardware models can offer a limited range of functions taken from all three of these device types, most often in the form of multiple built-in ethernet ports. However, it’s worth noting that even when certain features of a router, hub and network switch are combined into a single device, the capabilities and roles of each remain technically distinct from one another.

    What Speeds Can Network Switches Handle?

    When trying to pick the best ethernet switch for a given set of networking requirements, most suppliers and manufacturers tend to list their products according to one of three or more general speed categories. These are:

    • Fast Ethernet switches (FS) - 10/100 Mbps (standard IEEE 802.3u)
    • Gigabit network switches (GS or JGS) - 10/100/1000 Mbps (standard IEEE 802.3-2008)
    • Ten-gigabit network switches (GSS) - 10/100/1000/10000 Mbps (standard IEEE 802.3a)

    You may also see various other ethernet speeds and standards noted, such as 2.5 Gbps, 5 Gbps, 25 Gbps, 40 Gbps, 50 Gbps or 100 Gbps. These tend to be developed for more specialised applications.

    It is worth keeping in mind that the best network switch for domestic use isn’t necessarily going to be the best network switch for small business, industrial, or enterprise purposes.

    In fact, each of these applications will have considerably different requirements to consider, largely depending on the scale and speed of connectivity you need to create a stable and strong-performing network. While speed is always an important consideration, another key specification is the number of ports the specific switch offers.

    More ports mean greater flexibility across the network, but the amount of traffic able to flow through the network at any one time - in other words, the number of connected devices and users a network can comfortably support - will be limited by various factors, not least the bandwidth of your internet connection.

    How Many Network Switch Ports Do You Need for Your Network?

    In trying to decide how many network switch ports a particular setup requires for optimal convenience and performance, it’s wise to consider the following factors:

    • How many wired devices you want to connect, bearing in mind potential future device purchases
    • How much you are willing to spend on a network switch
    • Whether you would prefer to use a managed or unmanaged switch
    • Whether you require or can make use of advanced PoE models (either now or in the future)
    • What sort of bandwidth your current router and/or internet connection can comfortably support, and whether you may need to upgrade

    Popular choices for home networking often include small-to-medium sized hubs, such as 4-port5-port or 8-port network switches. Meanwhile, while more complex enterprise or server networks may require far more capable hardware such as a 64-port PoE switch.

    Popular Network Switch Brands

    Some of the most popular brands known for the quality, reliability, and advanced functionality of their network switches and related products include:

    FAQs