Press Releases
Affordable Renesas MCU prototyping boards now available from RS Components
Gadget Renesas SAKURA II development boards deliver flexible platform for range of applications including robotics and the IoT
Malaysia, 8 December 2016:
RS Components (RS), the trading brand of Electrocomponents plc (LSE:ECM), the global distributor for engineers, has announced availability of the Gadget Renesas SAKURA boards, which offer an easy-to-use development platform based on the Renesas RX family of flash microcontrollers. These general-purpose programmable boards offer a highly flexible platform that is suitable for a range of levels of software development experience from beginners at school to professional design engineers.
Gadget Renesas is a project concept developed by Renesas, which links ideas and electronics by providing boards that enable rapid prototyping and the sharing of ideas via its online community. It is ideal for use in developing projects across a range of applications in industrial, consumer and office automation, as well as in robotics and the Internet of Things (IoT).
The GR-SAKURA-II and GR-SAKURA-II-FULL development boards are based on the 32-bit RX63N microcontroller, specifically the R5F563NBDDFP in a 100-pin QFP package, with 1MB flash memory, 128KB RAM FPU and data flash of 32KB. The MCU operates at 3.3V and has a frequency of 96MHz (using an external 12MHz XO) with sub-clock speed of 32.768kHz. The RX63N microcontrollers are also supported by development software including a compiler online via the Renesas website, as well as software for developing Android smartphone applications.
The GR-SAKURA platform offers an Arduino compatible board footprint with C++ template and libraries and has Arduino UNO compatible pin-headers ready for use with Arduino shields. The boards also offer 51 GPIO pins, six analogue input pins, micro-SD jacket, XBee wireless module header footprints, JTAG interface, +5V DC power jack, user and reset switches, an Arduino Shield interface, and a range of interfaces including JTAG, mini-B USB-host connector and Ethernet.
The GR-SAKURA-II standard version is part populated with interface connectors, whereas the GR-SAKURA-FULL is fully populated with connectors, including: shield headers, RJ-45 Ethernet LAN connector, JTAG header, +5V DC power supply jack socket and a micro-SD card slot.
The Gadget Renesas SAKURA-II and SAKURA-FULL are shipping now from RS.
About RS Components
RS Components and Allied Electronics are the trading brands of Electrocomponents plc, the global distributor for engineers. With operations in 32 countries, we offer more than 500,000 products through the internet, catalogues and at trade counters to over one million customers, shipping more than 44,000 parcels a day. Our products, sourced from 2,500 leading suppliers, include electronic components, electrical, automation and control, and test and measurement equipment, and engineering tools and consumables.
Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2016 had revenues of £1.29bn.
For more information, please visit the website at www.rs-online.com.
Further information is available via these links:
Twitter: @RSElectronics; @alliedelec; @designsparkRS
RS Components on Linkedin
http://www.linkedin.com/company/rs-components
RS WeChat ID: RS_Components_CN
Relevant Links:
Electrocomponents plc
www.electrocomponents.com
RS Components
www.rs-online.com
DesignSpark
http://www.designspark.com