Press Releases


RS Components refreshes offering of pneumatic components from SMC with addition of more than 600 new products

Most extensive range of SMC pneumatics now available for new applications and maintenance of existing installations

Malaysia, 5 January 2016:

RS Components (RS), the trading brand of Electrocomponents plc (LSE:ECM), the global distributor for engineers, has announced a significant extension to its range of pneumatic components from SMC. Targeting machine builders developing new pneumatics-based applications as well as maintenance engineers, the additions to the SMC pneumatic components range comprise more than 600 products including cylinders, actuators, valves, fittings, assemblies, filters, lubricators, regulators, hoses and air-preparation devices.

Pneumatics technologies are deployed in a multitude of industry sectors including automotive, electronics, photovoltaics, print, pulp and paper, food and beverage processing, mineral processing and quarrying, and also in life sciences. RS is now the only global distributor holding stock for the majority of SMC pneumatic component products.

The increased range now includes the KQG2 one-touch pneumatic fittings manufactured from SUS316 stainless steel, which offers higher pitting and corrosion resistance. They are suitable for use with compressed air, water and steam, and are able to perform across a wide range of pressures from –100kPa up to 1MPa and temperatures from –5 up to +150°C.

Ideal for the food and beverage as well as the chemical industry, the devices include: straight, elbow and bulkhead threaded-to-tube adaptors, and straight, elbow, tee, and bulkhead tube-to-tube adaptors, tubing nuts and plugs for pneumatic adaptors and fittings, and elbow threaded adaptors. The KQG2 range of lightweight and compact push-in fittings are 30% smaller and 62% lighter than the existing KQG range and available to tubing diameters from 3.2 to 16mm.

Another highlight of the range is the new AR-B series of pneumatic air regulators. These offer pressure settings of either 0.05 to 0.7MPa or 0.02 to 0.2MPa, and feature a new lightweight modular design that allows connection to other SMC air-preparation equipment. The AR-B series can be mounted using a bracket, or can be panel mounted. All versions come with a locking setting nut to prevent accidental adjustment and are available in various body sizes (20 to 40) and with 1/8 to 1/2in piping.

Finally, the CP96 range of double and single acting ISO-cylinders provides a large number of options including 32 to 100mm bore, 25 to 500 mm stroke, and double and single rods. To eliminate piston rod lurching at the end of the stroke, the CP96 double-acting cylinders incorporate a floating seal mechanism and use precision bushings and piston-rod tolerances. Additional features include: fully adjustable end-of-stroke cushioning using a hex key; magnetic position sensing as standard; improved mounting accuracy; and a lightweight-profile barrel design.

The extensive range of pneumatic components and products from SMC is now available from RS in the EMEA and Asia Pacific regions.

About RS Components

RS Components and Allied Electronics are the trading brands of Electrocomponents plc, the global distributor for engineers. With operations in 32 countries, we offer more than 500,000 products through the internet, catalogues and at trade counters to over one million customers, shipping around 44,000 parcels a day. Our products, sourced from 2,500 leading suppliers, include electronic components, electrical, automation and control, and test and measurement equipment, and engineering tools and consumables.

Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2015 had revenues of £1.27bn.

For more information, please visit the website at www.rs-online.com.

Further information is available via these links:

Twitter: @RSElectronics; @alliedelec; @designsparkRS

RS Components on Linkedin
http://www.linkedin.com/company/rs-components

Relevant Links:

Electrocomponents plc
www.electrocomponents.com

RS Components
www.rs-online.com

DesignSpark
http://www.designspark.com