Press Releases
RS Components augments rapid-prototyping product portfolio with new Ultimaker 2 3D printer
High resolution, high speed and most popular 3D desktop printer available targets wide range of users including engineers involved in rapid-prototyping and product concept development
Kuala Lumpur, Malaysia, 20 November 2014:
RS Components (RS), the trading brand of Electrocomponents plc (LSE:ECM), the global distributor for engineers, has added to its growing range of rapid-prototyping machines with the Ultimaker 2 3D printer, recently voted Best Consumer Product 2014 at the London 3D Print Show Global Awards. This new desktop 3D printer employs fused filament fabrication (FFF) technology and targets electronics and mechanical engineers involved in design, prototyping and research and development, as well as enthusiasts and students.
Manufactured from premium parts and materials the latest version of the Ultimaker 3D printer, compared to its previous incarnation, now adds a heated bed, which smoothens the print output, allows for ABS material printing and also prevents warping. Claiming the highest speed and accuracy possible on any desktop 3D printer available today, the printer offers a print speed of up to 300mm/s and a layer resolution of only 20 microns or 0.02mm. In addition, it is available in a highly compact design with frame dimensions of 357 x 342 x 388mm (not including filament spool), offering an overall build volume of 230 x 225 x 205mm.
Other specifications include a nozzle diameter of 0.4mm, with the capability to handle a recommended filament diameter of 2.85mm. Operating temperatures of the print nozzle and heated bed are +180 – 260°C and +50 – 100°C, respectively.
Approximate usage cost, provided by the manufacturer Ultimaker, is €0.05 per cubic centimetre, combining both material and power cost. The use of FFF technology also allows the choice of a wide range of material filaments including popular choices such as PLA and ABS.
The printer also comes with a standalone SD-card for 3D-model file upload and Ultimaker’s Cura open-source software, which essentially slices a 3D-model into the requisite layers in preparation for printing. Cura was voted Best Consumer Software 2014 also at the London 3D Print Show Global Awards.
The Ultimaker 2 is available now from RS Components in EMEA and some Asia Pacific regions priced at MYR9,075.
About RS Components
RS Components and Allied Electronics are the trading brands of Electrocomponents plc, the global distributor for engineers. With operations in 32 countries, we offer around 500,000 products through the internet, catalogues and at trade counters to over one million customers, shipping more than 44,000 parcels a day. Our products, sourced from 2,500 leading suppliers, include semiconductors, interconnect, passives and electromechanical, automation and control, electrical, test and measurement, tools and consumables.
Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2014 had revenues of £1.27bn.
For more information, please visit the website at //www.rs-online.com
Further information is available via these links:
Twitter: @RSElectronics; @alliedelec; @designsparkRS
RS Components on Linkedin
http://www.linkedin.com/company/rs-components
Relevant Links:
Electrocomponents plc
www.electrocomponents.com
RS Components
www.rs-online.com
DesignSpark
http://www.designspark.com