Press Releases
Space-saving Modular PLC Available from RS Components Offers Scalable and Flexible Design for Small Automation Systems
The Siemens Simatic S7-1200 controller combines powerful integrated technology and a communications interface to provide fast start-up, precise monitoring and ease-of-use in automation tasks
Kuala Lumpur, Malaysia, 23 September 2014 :
RS Components (RS), the trading brand of Electrocomponents plc (LSE:ECM), the global distributor for engineers, has announced that, from October 2014, the popular Simatic S7-200 programmable logic controller (PLC) from Siemens is to be discontinued and fully replaced by the new generation Micro-SPS Simatic S7-1200 controller, which offers significant price and performance advantages over the previous model.
The compact Simatic S7-1200 controller has been engineered to reflect the growing importance of flexibility, modularity and scalability in hardware design, while providing powerful integrated functions that are easy to use. It offers five CPU types with different performance ratings and a modular design that can be expanded with additional inputs and outputs. The system can be finely scaled by installing 'signal boards' on an interface directly on the CPU to add a few digital or analogue channels, thus reducing space requirements in the control cabinet. The inputs and outputs of the CPU are also designed for motion control applications so that flexibility is already integrated in the basic module. Integrated technology functions include PID closed-loop control, motion and axis control.
The Simatic S7-1200 controller is configured with the STEP 7 Basic engineering software in the TIA Portal (Totally Integrated Automation). This means users have access to a standardised, comprehensive engineering tool for logic operations, HMI and networking with one shared editor. The entire navigation, all symbols and menus are standardised in all views, which makes the software easy to learn and use.
The S7-1200 features an integrated Profinet interface, which is standard in all CPUs and designed as a 2-port switch interface in the larger models, and supports distributed architectures with inputs and outputs, HMI, drives and other Profinet field devices. This feature is particularly useful if the controller operates in a networked system or if more than one HMI device is to be connected. Separate expansion modules are available for Profibus communication.
In addition, a GPRS module supports remote access from almost any location in the plant. This is useful during plant service, enabling faults to be eliminated remotely and service personnel to obtain information from transmitted diagnostics in advance, or order hardware components prior to the service call.
The Siemens Simatic S7-1200 PLC is available to purchase from RS stock globally.
About RS Components
RS Components and Allied Electronics are the trading brands of Electrocomponents plc, the global distributor for engineers. With operations in 32 countries, we offer around 500,000 products through the internet, catalogues and at trade counters to over one million customers, shipping more than 44,000 parcels a day. Our products, sourced from 2,500 leading suppliers, include semiconductors, interconnect, passives and electromechanical, automation and control, electrical, test and measurement, tools and consumables.
Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2014 had revenues of £1.27bn.
For more information, please visit the website at //www.rs-online.com
Further information is available via these links:
Twitter: @RSElectronics; @alliedelec; @designsparkRS
RS Components on Linkedin
http://www.linkedin.com/company/rs-components
Relevant Links:
Electrocomponents plc
www.electrocomponents.com
RS Components
www.rs-online.com
DesignSpark
http://www.designspark.com