Press Releases
RS Components Begins Distribution of Second-generation RepRapPro Ormerod, Bringing Affordable 3D Printing Technology to Engineers Worldwide
- RS first to supply complete kit to build new Ormerod 2 low-cost self-replicating 3D printer
- New open-source hardware design means easier assembly and performance improvements
- When combined with free DesignSpark Mechanical 3D design software it provides a further boost to rapid prototyping for all engineers
Kuala Lumpur, Malaysia, 18 September 2014 :
RS Components (RS), the trading brand of Electrocomponents plc (LSE: ECM), the global distributor for engineers, today announced availability of the new version of the RepRapPro Ormerod 3D printer which offers extensive versatility and functionality in an easy-to-assemble kit of parts. 3D printing enables electronic and mechanical engineers to quickly and easily realise early design concepts by creating fast-turnaround prototypes, potentially saving months in the product design cycle.
The RepRapPro Ormerod 2 is a single-colour low-cost 3D printing machine that is a full open-source and self-replicating RepRap and is one of the most versatile 3D printers available: it is easy to expand in functionality, fast to replicate and fast to assemble. All the RepRapPro printers, including previous machines such as the Ormerod and Mendel, are capable of self-replicating their own plastic components.
The Ormerod 2 brings several advantages compared to its predecessor, including a much simpler and more integrated assembly with improved instructions and wiring looms for simple plugin connection and no soldering necessary.
Other improvements come in the areas of the build bed, the y-carriage design, bed probe, extruder and power supply, as well as better emissions control and software support. For example, the Ormerod 2 design offers much easier adjustment of the bed level; improved y-axis belt location and retention delivers easier adjustment of belt tension; and a new bed probe now features a four-wire differential device, as well as providing much easier access to the extruder for cleaning purposes. In addition, the power supply is now a 100-240V worldwide input power supply and is a dedicated 12V supply, rather than being an adapted supply, and is more compact with its integration into the machine with no trailing wires. EMI emissions have also been reduced, resulting from a fully shielded design that meets the Class A CE mark.
Specifications of the Ormerod 2 printer include: build volume and speed of 200 x 200 x 200mm and 1800mm/min, respectively; a deposition rate of 33cm3 per hour; accuracy and layer resolution of 0.1mm and 0.01mm, respectively; and ability to print using either PLA or ABS thermoplastic materials. The open-source software designed to run the machine is fully compatible with the original Ormerod printer and will run on a relatively low powered computer running Windows, Linux/Ubuntu or Mac OS.
The RepRapPro Ormerod 2 is shipped ready for assembly as a kit of parts containing all the required components. The complete kit includes: all printed parts; all hardware, including threaded and smooth rods, screws, nuts, washers, belts and bearings; pre-soldered and programmed electronics; MicroSD card and adapter; heated PCB build surface; motors; nozzle assembly and extruder drive mechanism; 100m of 1.75mm-diameter white PLA filament material (weighing approximately 300g); a 100-240V worldwide input power supply (plugs available for EU, UK, US and Australia); plus open-source software to run the machine including firmware for the electronics.
"The availability of the second generation Ormerod 3D printing kit and latest in a line of RepRapPro 3D printers demonstrates the significant success of its open source self-replicating concept," said Mark Cundle, Head of Technical Marketing at RS Components. "Using this exciting and low-cost 3D printing technology, in conjunction with the free and intuitive DesignSpark Mechanical 3D design software and the library of 3D component models from RS, means that 3D design and rapid prototyping is becoming increasingly available to a much wider universe of designers and mechanical and electronics engineers. This can enable significant savings in product development cycles and mean much faster time-to-market."
Like the first Ormerod, the Ormerod 2 uses the FFF (Fused Filament Fabrication) process, which can build 3D objects in a range of plastics and also in a variety of colours. The process enables the creation of almost any shape that can be modelled on a computer, including some that cannot be produced by traditional manufacturing techniques. 3D printing is fast becoming an essential part of the electronic and mechanical design process. Increasing numbers of companies are beginning to see the benefits of using this technology to create quick-turn-around prototypes and save months in the design cycle. Barriers to adoption in the past have been the cost of hardware and a lack of easy-to-use design software for non-CAD specialists. However, when used in conjunction with the free DesignSpark Mechanical 3D modelling software, the Ormerod 2 3D printing kit will enable design engineers around the world to develop sophisticated concepts and products very quickly and inexpensively.
The RepRapPro Ormerod 2 is now in stock at RS Components, priced at MYR 2,880.21, as a kit of parts containing all the components required for full assembly.
About RS Components
RS Components and Allied Electronics are the trading brands of Electrocomponents plc, the global distributor for engineers. With operations in 32 countries, we offer around 500,000 products through the internet, catalogues and at trade counters to over one million customers, shipping more than 44,000 parcels a day. Our products, sourced from 2,500 leading suppliers, include semiconductors, interconnect, passives and electromechanical, automation and control, electrical, test and measurement, tools and consumables.
Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2014 had revenues of £1.27bn.
For more information, please visit the website at //www.rs-online.com
Further information is available via these links:
Twitter: @RSElectronics; @alliedelec; @designsparkRS
RS Components on Linkedin
http://www.linkedin.com/company/rs-components
Relevant Links:
Electrocomponents plc
www.electrocomponents.com
RS Components
www.rs-online.com
DesignSpark
http://www.designspark.com