Press Releases
ISO-TECH High-reliability and Cost-effective Clamp Meters from RS Components Enable Safe and Fast Current Measurements
Ideal for use by electricians and maintenance professionals, ergonomically designed and easy-to-use multimeters also provide highly accurate voltage and resistance measurement and continuity testing
Malaysia, 26 August 2014 :
RS Components (RS), the trading brand of Electrocomponents plc (LSE:ECM), the world's leading high service distributor of electronics and maintenance products, has announced availability of two new high-reliability clamp meter products that are designed for making safe and non-intrusive current measurements in a range of electrical, panel and equipment maintenance applications.
Clamp meters are ideal tools for making spot checks and verifying system conditions before deploying more specialised tools and incurring additional costs. The compact and ergonomically designed ISO-TECH ILCM03A and ICM30R clamp meters come at prices that are approximately 30% cheaper than leading brands and are must-have devices for any electrician's or maintenance professional's toolbox.
The ILCM03A is primarily geared toward current leakage detection, while a key feature of the ICM30R is its ability to make true-RMS AC current readings. Both devices also offer reliable and accurate voltage and resistance measurements as well as continuity testing for circuit breaks.
The ILCM03A clamp meter is a highly portable device with compact dimensions of only 210 x 62 x 35.6mm. It also has a single large rotary function-selection switch enabling one-handed measurement and a large backlight 3.75-digit LCD with an analogue bar graph, making it a tool that is easy to use and easy to read in any environment. The meter also offers a large-jaw design that enables non-intrusive current measurement on cables and wires that are up to 30mm in diameter.
The ICM30R clamp meter integrates dual Hall sensors to provide reliable and accurate current measurements, and provides the true-RMS AC current value of both pure and distorted waveforms. The meter is also a highly portable and easy-to-use and -read device that features a special hand-guard design, which provides additional user protection that prevents direct contact with electrical conductors.
Manufactured and tested to international standards, both ISO-TECH clamp meters are rated to CAT II 600V and CAT III 300V, according to IEC 61010. The meters come with a three-year warranty and are available to purchase direct from RS stock globally. For more information please visit www.iso-techonline.com.
About RS Components
RS Components and Allied Electronics are the trading brands of Electrocomponents plc, the global distributor for engineers. With operations in 32 countries, we offer around 500,000 products through the internet, catalogues and at trade counters to over one million customers, shipping more than 44,000 parcels a day. Our products, sourced from 2,500 leading suppliers, include semiconductors, interconnect, passives and electromechanical, automation and control, electrical, test and measurement, tools and consumables.
Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2014 had revenues of £1.27bn.
For more information, please visit the website at //www.rs-online.com
Further information is available via these links:
Twitter: @RSElectronics; @alliedelec; @designsparkRS
RS Components on Linkedin
http://www.linkedin.com/company/rs-components
Relevant Links:
Electrocomponents plc
www.electrocomponents.com
RS Components
www.rs-online.com
DesignSpark
http://www.designspark.com