Press Releases
RS Components expands wireless connectivity solutions for Raspberry Pi
Latest Raspberry Pi products available from RS feature Wi-Fi and RF technology to provide low cost, low power wireless functionality
Malaysia, 31 March 2014 :
RS Components (RS), the trading brand of Electrocomponents plc (LSE:ECM), the world’s leading high service distributor of electronics and maintenance products, has added two wireless connectivity options to its growing portfolio of products based on the Raspberry Pi computer. The new modules are built using Wi-Fi and low power radio technology respectively and deliver wireless interface capability for applications requiring low cost, low power, small form factor solutions, such as mobile devices.
The first module, a wireless nano USB adapter from Edimax, provides high-speed Wi-Fi functionality compliant with the IEEE802.11b/g/n wireless protocol via a tiny adapter that plugs into the USB port on the Raspberry Pi. The adapter supports transmission rates of up to 150Mbps, which is ideal for large data transfer and three times faster than standard 11g connections. The smart adapter adjusts the transmission output according to the distance and CPU offload to achieve a reduction in power consumption of between 20% and 50% when the wireless function is idle. It can be configured using Wi-Fi Protected Setup (WPS) to provide a simple, secure wireless network.
The second module, Connect2Pi from LPRS, also features a USB wireless device offering ‘plug-and-play’ connection to the Raspberry Pi, but instead uses low power RF transceiver technology to provide a bi-directional link to any device supporting serial communications, for example another Raspberry Pi. Frequency, bandwidth, power output and data rates can be configured to allow multiple devices to communicate free from interference from each other and any other RF devices. The RF technology employed enables significantly greater range (up to 200m depending on the terrain) and lower power consumption than other wireless protocols such as Wi-Fi or Bluetooth. The host device can send and receive up to 180 Bytes of data per packet to other hosts within range, making it particularly useful for ‘sense and control’ applications. 433MHz and 868MHz versions are available and an integral SMA antenna is included. A kit variant of this product is also available, which contains dual rather than a single transceiver.
All three Raspberry Pi wireless products are available to purchase from RS stock for same-day despatch.
About RS Components
RS Components and Allied Electronics are the trading brands of Electrocomponents plc, the world's leading high service distributor of electronics and maintenance products. With operations in 32 countries, we offer around 500,000 products through the internet, catalogues and at trade counters to over one million customers, shipping around 44,000 parcels a day. Our products, sourced from 2,500 leading suppliers, include electronics, automation and control, test and measurement, electrical and mechanical components.
Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2013 had revenues of GBP1.24bn.
For more information, please visit the website at http://www.rs-components.com.
Further information is available via these links:
Twitter: @RSElectronics; @alliedelec; @designsparkRS
RS Components on Linkedin
http://www.linkedin.com/company/rs-components
Relevant Links:
Electrocomponents plc
www.electrocomponents.com
RS Components
www.rs-components.com
DesignSpark
http://www.designspark.com